キーワード、オーダーコード、製品コード、またはシリアル番号で検索してください(例:「CM442」や「技術仕様書」)
2 文字以上を入力して検索を開始してください。

Close cooperation brings results

Endress+Hauser and Boliden Kokkola developed density measurement to the highest level

New technology was needed for the sludge density measurement of Boliden Kokkola’s zinc plant. In the development cooperation, the expertise of Endress+Hauser and Boliden experts as well as the Thesis worker’s skills were utilized.

Endress+Hauser and Boliden Kokkola developed density measurement to the highest level

Boliden Kokkola’s sludge density measurement

  • A critical part of the zinc refining process and filtration of ferrous jarosite precipitate.

  • Implemented with Endress+Hauser’s Vibronic Point level detection Liquiphant FTL51C measurement.

  • A vibrating level measurement solution that detects even minor variations in the density of the medium. The 1.5-metre sensor is connected to Endress+Hauser’s calculation unit.

  • The PFA-coated sensor is resistant to surface sediment.

  • Also suitable for measuring solutions with variable density in other industries.

Boliden Kokkola wanted to improve density measurement in the jarosite supply tank, from which the sludge containing iron precipitate is directed to filtration. Balancing the density in the tank also balances the strength of the solids layer on the six belt filters.

“The aim is to use density measurements in daily process operation so that the solution coming from the belt filters has been filtered as effectively as possible to contain the desirable components such as water-soluble zinc, which should conversely be minimized in the outgoing jarosite precipitate,” says Boliden Kokkola’s Automation Specialist Matti Karjula.

A decision was made to implement the measurement with Endress+Hauser’s vibrating level switch and density calculator

“Endress+Hauser had good references with corresponding measurement positions. Based on them, we suggested a solution which fortunately also convinced the customer,” says Kari Isometsä, Endress+Hauser’s Manager for Northern Finland.

Important data to support the choice of equipment was gained from the thesis of process, material and chemical technology engineer Noora Alapiha in which she examined the functioning of the density measurement.

The development cooperation was worth the effort

Ideally cooperation leads to results and benefits that stand the test of time. Both Boliden and Endress+Hauser are extremely pleased with how the right measurement technology enables clear savings in the treatment process.

“The precise density measurement enables optimizing the capacity of the sludge to be treated and the amount of chemicals needed for the reaction. This, in turn, guarantees a better treatment result, which ensures cleaner process waste and more recovered zinc,” Karjula says.

お問い合わせ先

当社の製品にご興味をお持ちですか?ご使用のアプリケーションについてご相談がおありですか?

お問合せ、お困りごとの内容はできるだけ詳しくお知らせください。より適切なサポートが可能になります。

  • シンプルな製品

  • 選定、設置、操作が簡単

技術的卓越性

シンプルさ

  • 標準的製品

  • 高い信頼性と堅牢性、容易なメンテナンス

技術的卓越性

シンプルさ

  • ハイエンド製品

  • 高性能で高い利便性

技術的卓越性

シンプルさ

  • 特殊仕様の製品

  • 要件の厳しいアプリケーション向けに設計

技術的卓越性

シンプルさ

高い柔軟性

FLEX セレクション 技術的卓越性 シンプルさ
  • F
  • L
  • E
  • X

Fundamental セレクション

基本的な測定要件に対応

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Lean セレクション

コアプロセスの要件に対応

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Extended セレクション

革新的な技術でプロセスを最適化

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Xpert セレクション

最も困難なアプリケーションにも対応

技術的卓越性
シンプルさ

高い柔軟性