キーワード、オーダーコード、製品コード、またはシリアル番号で検索してください(例:「CM442」や「技術仕様書」)
2 文字以上を入力して検索を開始してください。

Sustainable progress with innovative measurement technology

Flensburger combines tradition with modern process precision

For Flensburger Brauerei, sustainability is not a minor matter, but a central corporate objective. The brewery relies on innovative technologies in order to produce in a resource-saving manner and at the same time guarantee the highest beer quality.

Constructive exchange between brewery experts ©Endress+Hauser

Constructive exchange desired: Jan Henrik Bernhardt from Endress+Hauser in conversation with master brewer Enes Erisgen

Video Flensburger Brauerei - Innovative measurment technology for sustainable brewing

Results

  • Inline measuring technology for fermentation monitoring: Extract values and fermentation parameters are seamlessly recorded directly in the tank

  • Continuous measurement of the COD content in wastewater provides clarity about wastewater flows and their pollution

  • Decisive steps towards conserving resources, saving money and achieving sustainability goals

Brew master Enes Erisgen, Flensburger Brauerei

"The issue of sustainability is a major challenge for the brewery. As Flensburger Brauerei, we are always looking for someone to enter into discussions in order to make progress together in the end."

Enes Erisgen, Master brewer of Flensburger Brauerei
Flensburger Brauerei Emil Petersen GmbH & Co. KG

Challenges

For Flensburger Brauerei to achieve its sustainability goals, the brewing process must be viewed holistically. It's not just about efficiency and product quality in the actual fermentation and brewing process, but also about the downstream steps. It is particularly important to reduce drinking water consumption, reduce wastewater volumes and use the resulting wastewater as an energy source and for the reuse of existing resources.

Realization

A tailor-made solution for optimizing the processes in the fermentation cellar was jointly developed to meet the challenges of the brewing process. At its heart is the QWX43 Fermentation Monitor, which enables continuous monitoring and control of fermentation.

Precise measurement technology for the targeted treatment and reuse of wastewater. Here, Memosens Wave CAS80E ensures that the wastewater volumes are fed to the correct process stages in future.

お問い合わせ先

当社の製品にご興味をお持ちですか?ご使用のアプリケーションについてご相談がおありですか?

お問合せ、お困りごとの内容はできるだけ詳しくお知らせください。より適切なサポートが可能になります。

  • シンプルな製品

  • 選定、設置、操作が簡単

技術的卓越性

シンプルさ

  • 標準的製品

  • 高い信頼性と堅牢性、容易なメンテナンス

技術的卓越性

シンプルさ

  • ハイエンド製品

  • 高性能で高い利便性

技術的卓越性

シンプルさ

  • 特殊仕様の製品

  • 要件の厳しいアプリケーション向けに設計

技術的卓越性

シンプルさ

高い柔軟性

FLEX セレクション 技術的卓越性 シンプルさ
  • F
  • L
  • E
  • X

Fundamental セレクション

基本的な測定要件に対応

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Lean セレクション

コアプロセスの要件に対応

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Extended セレクション

革新的な技術でプロセスを最適化

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Xpert セレクション

最も困難なアプリケーションにも対応

技術的卓越性
シンプルさ

高い柔軟性