Title

キーワード、オーダーコード、製品コード、またはシリアル番号で検索してください(例:「CM442」や「技術仕様書」)
2 文字以上を入力して検索を開始してください。

From the laboratory to the field with Raman spectroscopy

Evonik's scalable PAT solution – for greater efficiency, safety, and quality in specialty chemicals manufacturing

>インダストリ: 化学産業
Process Engineer and Endress+Hauser Raman probe at Evonik

概要

In partnership with Endress+Hauser, Evonik has successfully integrated Raman spectroscopy as a powerful process analysis technology (PAT) from the laboratory to pilot plants, right through to production. This technology delivers real-time data, increases efficiency, reduces costs, and improves product quality. Its flexibility, scalability, and safety make it the key to new savings potential in chemical process development. Customers can benefit directly from this acquired expertise to optimize their own development and production processes in a sustainable manner.

The results: Greater efficiency, safety, and quality

16

installed Raman Rxn2 analyzers

50+

measuring points with Raman Rxn probes

Raman spectroscopy from Endress+Hauser has established itself as a key PAT tool at Evonik. It enables significant efficiency gains, cost reductions, and faster market launch of new products.

Results include:

  • End-to-end process analysis from the laboratory to production
  • Real-time measurements possible at several measuring points at the same time
  • Inline measurements replace manual sampling
  • Suitability for pilot plants with low volumes
  • Reliable operation even under difficult conditions (e.g., ATEX zones)
  • Reduction in the time to market
  • Cost reduction through elimination of laboratory evaluations and reduced personnel costs
  • Increased safety
  • Internal acceptance and acquisition of expertise
Photo of Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

"With Raman spectra, you might be able to assign isolated peaks to individual substances in the mixture. This significantly reduces the calibration effort and quickly leads to quantitative results."

Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG

The challenge: Find a versatile, real-time lab-to-process solution

Back in 2016, Evonik launched its company-wide “lab to process” strategy with the aim of embedding PAT technologies early on in process development. Evonik was looking for a process analysis technology that would efficiently support the entire development and optimization process while also helping to reduce costs. The goal was to find a solution that not only provides accurate real-time data but is also versatile enough to be used in a wide variety of process environments – from the laboratory to production.

The technology should:

  • be universally applicable for a wide range of chemicals, states of matter and process conditions
  • be flexible and scalable from the R&D lab to large-scale production facilities
  • be quick to integrate in order to shorten development times and reduce time to market
  • improve product quality through continuous inline measurements
  • function reliably even under demanding conditions such as ATEX zones

Our solution: A scalable PAT Endress+Hauser Raman spectroscopy system

Endress+Hauser provided Evonik with a customized solution based on Raman spectroscopy – a technology that meets all of the requirements outlined. The systems are characterized by their exceptional modularity and versatility. Thanks to optical fibers and various probe types, they can be easily integrated into a wide variety of installation situations. Up to four independent channels enable simultaneous monitoring of multiple measuring points – a clear advantage for complex processes.

The chemometric suitability of the spectra offers particular added value – due to compatibility with all common chemometric programs, these can be analyzed directly on the spectrometer in a way that is versatile, intuitive, and achieved in real time. This allows qualitative and quantitative data to be recorded and interpreted immediately during the process – without any time-consuming manual sampling.

Raman spectroscopy was successfully used for the first time in a pilot plant for the development of hydrogenation processes. The probe was integrated into a 6 mm pipe – significantly smaller than in production facilities. Instead of daily NMR sampling, the technology now enables inline measurements to be taken every single minute, and the process continuously monitored.

This process is efficient, precise, and safe. In pilot plants with low volumes in particular, the system composition remains unchanged because no samples need to be taken. This not only saves time and money but also increases safety for both personnel and plant.

Hazardous area use

Thanks to its standardized and certified components, the Raman system can even be used in ATEX zones at a cost that is reasonable. For use in potentially explosive atmospheres, Evonik also uses the Liquiphant Vibronic level switch. This ensures that no flammable gas mixture can form in the laser beam of the Raman probe – a decisive contribution to process safety.

Testimonial

Photo of Dr. Roland Peschke, PAT expert at specialty chemical manufacturer Evonik

“The requirements for PAT measurement systems are particularly high, especially in the harsh environment of process plants and the need to comply with ATEX regulations. Raman spectroscopy has established itself as a robust and reliable tool in this area.” - Dr. Roland Peschke, PAT expert at Evonik Oxeno

Global roll out

This system has enabled Evonik not only to increase efficiency and quality in process development, but also to successfully transfer technology from the laboratory to production – a real key to new savings potential. Following successful implementation in Germany, Raman technology is now being rolled out internationally in Evonik’s first production plants – supported by the global expertise of Endress+Hauser.

Free download

Download the case study

Want access to the full case study as a PDF? Download a copy to read at your convenience, save for future reference, or share with colleagues.

Download the case study

お問い合わせ先

>当社の製品にご興味をお持ちですか?ご使用のアプリケーションについてご相談がおありですか?

お問合せ、お困りごとの内容はできるだけ詳しくお知らせください。より適切なサポートが可能になります。

Products and services used

/

Related solutions and technology

化学成分の光学式分析

固体からガスまで、組成や濃度を測定・監視する光学式分析システム。研究室、製造プロセス、排出監視に対応。

詳細情報

排水放流の監視 

測定値を確実かつ包括的に継続監視し、汚染に迅速に対応することで、法定限度値を遵守しながら排水を放流します。

詳細を見る

天然ガスパイプライン内の水素測定

ラマン分光法を用いた天然ガスパイプラインにおける水素の高速連続測定により、消耗品やフレアリングを必要とせずに、安全な混合、品質基準への適合、ダイナミックな制御が可能

続きを読む

基準に適合した安全なガス注入のためのバイオメタン品質分析 

H₂Sや水露点をはじめ、ガスグリッドへの安全な注入や効率的な運用にとって重要なパラメータを、迅速に高精度でオンライン測定することで、信頼性の高いバイオメタン品質を確保します。 

続きを読む

淡水化におけるオンライン水質モニタリングで逆浸透膜を保護 

淡水化と水の再利用の用途において、信頼性に優れたオンライン水質モニタリングにより、RO(逆浸透)膜を保護して、洗浄作業を軽減し、メンブレンを長寿命化

続きを読む

低温貯槽における漏れ検出(LNG、エチレン、LPG、アンモニア)

低温貯槽の漏れを早期に検出し、安全な運用を実現します。Endress+Hauserは、高信頼性の連続温度監視により、作業者、設備、重要インフラを保護します。

詳細を見る

CCUSのリアルタイム測定と検証

CO₂回収の未来を切り拓く:高密度相用途に対応した、高精度で信頼性の高いソリューション

さらに詳しく

規制要件への対応を支える連続排出監視ソリューション

規制要件への対応を支える連続排出監視ソリューション

詳細情報

FAQs

企業ロゴ: Evonik Industries AG

エボニック インダストリーズAGはドイツのEssenに本社を置く、スペシャルティケミカル分野のグローバルリーダーです。イノベーションと卓越した技術への情熱を礎に、同社は従来の化学の枠を超え、産業と社会に向けた持続可能なソリューションを創出しています。エボニックは、6つの大陸の27か国で製造拠点を運営しています。