Title

キーワード、オーダーコード、製品コード、またはシリアル番号で検索してください(例:「CM442」や「技術仕様書」)
2 文字以上を入力して検索を開始してください。

Waste-to-energy plant in Spain relies on proven technology for emission measurement

>インダストリ: 複数の業界
TERSA's sustainable Waste-to-energy plant in Barcelona

お問合せ、お困りごとの内容はできるだけ詳しくお知らせください。より適切なサポートが可能になります。

概要

A waste-to energy (WtE) plant in Sant Adrià del Besòs near Barcelona in Spain has rolled out an innovative system for ensuring better environmental practices. The plant is owned by the TERSA Group, a publicly owned environmental management company and designed for handling municipal waste. SICK Spain (now marketed by Endress+Hauser Spain) installed two measurement systems, doubling the reliability of the plant’s emissions data.

The results:

  • In line with the measures put in place by the local authorities to improve air quality, the TERSA Group aims to achieve the highest standards possible for efficiency and environmental sustainability. It believes that the new catalytic system installed in the WtE plant and driven by proven measurement technology is a key part of its efforts.
  • The project followed on from a public tendering procedure, which was won by PASCH, a Spanish company specializing in supplying and maintaining equipment.
  • This article was first published on www.sick.com on March 3rd, 2021. Since Jan 1st, 2025 Endress+Hauser exclusively markets SICK’s gas analysis and flow measurement technology worldwide.

The customer requirement: “We need the best emission monitoring solution available”

The plant has three waste treatment lines, with a maximum annual capacity of 360,000 tons, and annual production of 200,000 MW of electricity. “Because of where it is and what it does, the plant can potentially have a significant environmental impact. In order to ensure we meet levels set out in legal standards, we need the best emission measurement technology available”, explained Alessandro Leotta, Head of WtE at the TERSA Group.

Our solution:

With this goal in mind, the right environmental measurement equipment helps to improve process efficiency while minimizing the plant’s impact on the surrounding environment. This project involved a full analyzer system in the stack, along with a redundant system, designed to double the reliability of the data sent to the Catalonian authorities about the plant’s emissions.

These two pieces of equipment are made up of two MCS100FT multi-component Analyzers, two MERCEM300Z mercury Analyzers, two DUSTHUNTER SP100 particle Analyzers, two FLOWSIC100 gas flow measuring instruments, two MPR remote monitoring elements, and two control cabinets, along with a data handling system and another system used by both the plant and the local authorities to send the data. 

The equipment supply contract includes 24/7 maintenance, with a 4-hour response time. The system also has a remote monitoring service operated from Germany, which enhances the level of support.

During the lockdown caused by the COVID-19 pandemic, the MPR monitoring system has made it possible to diagnose faults, maintain the Analyzers, and manage alarms remotely, as well as the automated QAL3 settings. All of these features have contributed to helping the plant to keep operating and providing an essential service.

お問い合わせ先

>当社の製品にご興味をお持ちですか?ご使用のアプリケーションについてご相談がおありですか?

お問合せ、お困りごとの内容はできるだけ詳しくお知らせください。より適切なサポートが可能になります。

Products and services used

/

Related solutions and technology

排出ガス監視ソリューション

弊社の数十年にわたる経験と、継続的な排出ガス監視のための包括的な製品ランナップ、そしてお客様の産業のそれぞれの測定作業に合わせた未来志向のソリューションを活用してください。

詳細情報

粒子計測機器

環境の持続可能性を維持するには、排出される粉塵や粒子の検出と正確な測定が必要です。弊社の堅牢でメンテナンスの容易な機器により、粒子計測システムの新たな基準が打ち立てられます。

詳細情報

超音波流量計

Proline Prosonic FlowおよびFLOWSIC超音波センサーは、最大呼び口径4000A(156")までのガスおよび液体の多用途で経済的な測定を保証します。

詳細情報

プロセスガスアナライザ

重要な課題を解決するために、最新のガス分析とプロセス測定が産業界をサポートします。弊社の技術により、効率を高めるためのカスタマイズされたソリューションの共同開発が可能になります。

詳細情報

企業ロゴ: TERSA Group Waste-to energy plant

TERSA社はBarcelona都市圏で事業を展開する公営企業で、循環型経済に関連する環境サービスの管理を専門としています。事業活動を通じて、廃棄物管理や再生可能エネルギーの発電・販売における課題に対応するソリューションを提供し、市民による環境保全への取り組みも促進しています。TERSAグループは、TERSA社、SEMESA社、SIRESA社で構成されています。