キーワード、オーダーコード、製品コード、またはシリアル番号で検索してください(例:「CM442」や「技術仕様書」)
2 文字以上を入力して検索を開始してください。

Driving accuracy in space propulsion

Protolaunch uses flowmeters to test critical hardware for ambitious space missions

Protolaunch provides space propulsion expertise to commercial and international space agency partners. The company in Buckinghamshire (UK) has developed two types of rocket engines for spacecraft as well as supporting components, including valves for testing of the Rosalind Franklin Mars lander. On the ground, instrumentation from Endress+Hauser is used to demonstrate the performance of the propulsion systems and components.

Protolaunch undertakes cutting-edge propulsion testing from its facility in Westcott, UK

Flowmeters are used in rocket propulsion testing

Protolaunch undertakes cutting-edge propulsion testing from its facility in Westcott, UK

Protolaunch’s propulsion system HILBERT.

The result

  • Economic use of propellant on spacecraft thanks to ground tests demonstrating that the desired performance can be achieved for Protolaunch’s customers

  • High-performance flowmeters able to measure different media from water to oxygen/hydrogen and even nitrous oxide

  • Accurate results with fast response times

  • Efficient decision-making thanks to helpful tools to select and size instrumentation

  • Reliable expert support from Endress+Hauser

Picture of Dr Jack Coghen-Brewster, CTO, Protolaunch

"Endress+Hauser’s flowmeters work really well and we’ve had a lot of good interactions with the team."

Dr Jack Coghen-Brewster, CTO
Protolaunch

The customer requirement

When testing the flow of water, oxygen/hydrogen or nitrous oxide, accuracy and response time are crucial. “Our throttling valves are capable of actuating from zero to fully open in less than 100 milliseconds, so we need the flowmeter to respond as quickly as possible,” confirms CTO Dr Jack Coghen-Brewster. “Another key metric for propulsion systems is specific impulse, which is like miles per gallon for a car. Being able to accurately measure propellant delivery rates is critical.”

Our solution

Endress+Hauser was first brought in to supply instrumentation for a water rig, part of the development process to ensure the hardware works before bringing in expensive propellants. Since then, Endress+Hauser flowmeters have been used on many different types of media required for rocket engines. The Proline Promass E 300 Coriolis flowmeter, for example, has been employed to measure mass flow in the nitrous oxide propellant delivery system, and others have been used to measure propellant delivery rates.

Devices used

  • Proline Promass E 300 for direct measurement of mass flow in the nitrous oxide propellant delivery system

  • Proline Prowirl F 200 for monitoring propellant delivery rates and in calorimetry applications in conjunction with engine temperature readings to measure total rocket engine heat output

  • Liquiphant level sensors with high-level and low-level alarms are used in the propellant tanks

  • シンプルな製品

  • 選定、設置、操作が簡単

技術的卓越性

シンプルさ

  • 標準的製品

  • 高い信頼性と堅牢性、容易なメンテナンス

技術的卓越性

シンプルさ

  • ハイエンド製品

  • 高性能で高い利便性

技術的卓越性

シンプルさ

  • 特殊仕様の製品

  • 要件の厳しいアプリケーション向けに設計

技術的卓越性

シンプルさ

高い柔軟性

FLEX セレクション 技術的卓越性 シンプルさ
  • F
  • L
  • E
  • X

Fundamental セレクション

基本的な測定要件に対応

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Lean セレクション

コアプロセスの要件に対応

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Extended セレクション

革新的な技術でプロセスを最適化

技術的卓越性
シンプルさ
  • F
  • L
  • E
  • X

Xpert セレクション

最も困難なアプリケーションにも対応

技術的卓越性
シンプルさ

高い柔軟性